跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

The user's manual states on how to set FMR01 bit of FMR0 register. Why?

Latest Updated:03/08/2012

Question:

The user's manual states about how to set the FMR01 bit of the FMR0 register, "To set this bit to "1", write "0" and then "1" in succession". Why?

Answer:

 

This prevents easy rewrite. To set this bit to "1", set "0" once immediately before the instructions to set "1" and then set "1". The instructions should be as follows:

bclr bit_symbol
bset bit_symbol

Make sure no interrupts or DMA transfers are generated between these two instructions.

 
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N