跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

So the NEC format cannot be used without using custom code?

Latest Updated:04/01/2006

Question:

So the NEC format cannot be used without using custom code?

Answer:

No, the custom code's 00XXH section can be freely used.
However, there are risks when other devices use this same code.
Suitable Products