跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Should I do the manual screening for flash microcontrollers?

Latest Updated:02/01/2008

Question:

According to user's manuals, OTP microcontrollers were required to do manual screening after writing user's program in it, but in the case of flash microcontrollers, no mention is made of screening like that. Should I do the screening?

Answer:

In the case of flash microcontrollers, screening after writing your program in the flash microcontroller is not required.
Suitable Products