跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

SDA fixed low during I2C communication, R8C master

Latest Updated:09/30/2016

Question:

When carrying out I2C communication using an R8C device on the master side, sometimes the SDA line is fixed to low level and communication can't be carried out. How do I fix this situation?

Answer:

A clock discrepancy may occur between the master and slave due to noise, etc. on the SCL line of the I2C bus. This occurs due to differences in VIH/VIL characteristics or noise elimination capabilities of the two devices causing a difference in whether or not noise, etc. on the SCL line is recognized is a clock. For example, ACK output from the slave side could fix SDA to low level.

To release SDA from being fixed at low level from the slave side, switch the SCL/SDA pin of the R8C microcontroller on the master side to a general port, and output a pseudo-clock from the pin shared wth SCL (use high impedance and low level output to output a pseudo-clock). Then check whether SDA has been released on the slave side. If SDA has not been released yet, repeat this pseudo-clock output the slave side releases SDA. After the slave side releases SDA, return the setting on the master side to the I2C bus and issue a stop condition to end communication. For many slave devices, the I2C bus is initialized (reset) using a stop condition or a start condition. Depending on the slave device, the initialization method (reset method) may be described in the manual. In such cases, please initialize (reset) the slave device according to the description in the manual. For how to resolve SDA of an R8C device on the master side being fixed to low level, please refer to FAQNo:107183.

Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/3MK
R8C/34K
R8C/3MU
R8C/34U
R8C/3MQ
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
R8C/LA3A
R8C/LA5A
R8C/LA6A
R8C/LA8A