Ports P10-P15 (P10-P17 for 7549) set input mode; key-on for input to P10
Latest Updated:03/13/2008
Question:
(Interrupt) Can ports P10 to P15 (P10 to P17 for 7549) be set to input mode and key-on wakeup enabled only for input to P10? [2008/03/13]
Answer:
Yes.
Key-on wake up settings for each individual pin can be enabled and disabled using the key input control register. (#106882)
Key-on wake up settings for each individual pin can be enabled and disabled using the key input control register. (#106882)
Suitable Products
7548 |
7549 |