跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Ports P00-P07 set input mode; key-on for input to P00?

Latest Updated:11/05/2008

Question:

(Interrupt)  Can ports P00 to P07 be set to input mode and key-on wakeup enabled only for input to P00? [2008/11/05]

Answer:

Yes.
Key-on wakeup settings for each individual pin can be enabled and disabled using the key input control register. (#107007)
Suitable Products
7545