跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Microcomputer has no INTi. Can external interrupts be used?

Latest Updated:03/21/2017

Question:

The microcomputer used in our system apparently does not have external interrupt pins (INTi). Can I use external interrupts with the microcomputer?

Answer:

The TINi pin can be used as an external interrupt pin.
The TINi pin is shared with a multijunction timer input pin.
Suitable Products
32170, 32174
32171
32172, 32173
32176
32180
32182
32185
32186
32192
32195
32196
  • 本文是否實用?