跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is transition possible between high/medium speed modes when released

Latest Updated:01/18/2008

Question:

Is transition between high-speed/medium-speed modes possible while the external bus is released?

Answer:

Yes, transition is possible. While transitioning, the external bus will remain in high-impedance state.
Suitable Products
H8S/2655
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2556, 2552, 2506
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2339
H8S/2319
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2218, 2212
  • 本文是否實用?