跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is there any problem when real pins enter the open states?

Latest Updated:03/25/2009

Question:

When Pull-up MOS pins are set to the off-state from the on-states, the real pins enter the open states, is there any problem?

Answer:

There is no problem; you can solve this problem by setting the port register to "output pin and low level output", immediately after you make off-setting.
Suitable Products
H8/300H Tiny
H8/36087
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902
  • 本文是否實用?