跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is there I/O characteristic information?

Latest Updated:03/25/2009

Question:

Is there I/O characteristic information?

Answer:

You can download from the characteristic information page in this web site.

Please read the caution before using the characteristic information.

Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902