Is receive clock generated at fall of start bit and does delays occur?
Latest Updated:03/01/2005
Question:
(Serial Interface) Is the UART receive clock generated at the fall of the start bit? During a continuous receive, does a gradual delay of the receive clock occur? [2005/03/01]
Answer:
The receive clock is generated at the fall of the start bit. Consequently, a gradual delay of the receive clock does not occur during a continuous receive. (#104802)
Suitable Products
3803H |
3803L |
3823 |
3850A |
3858 |
38D2 |
38D5 |
7544 |
7546 |
7547 |
7548 |
7549 |