跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it prohibited to set 0000 to this register in uPD78P4038?

Latest Updated:02/01/2008

Question:

In the uPD78P4038, setting 0000 to the prescaler mode register is prohibited.
Does this mean that it is not OK to set 0000 to this register?

Answer:

Yes, that is correct.
Suitable Products
UPD78403x