跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it possible to return from watch mode without a sub-oscillator?

Latest Updated:03/25/2009

Question:

Is it possible to return from the watch mode, if transiting to watch mode without connecting any sub-oscillator?

Answer:

It is not recommended to transfer to the sub-clock type mode without connecting sub-oscillator. However, the external interrupt (IRQ0) or wake-up function enables to return from the watch mode.

In the case of connecting no sub-oscillator, be sure to fix X1 pin to GND.

 

Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power