跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it possible, output synchronous serial signal from V850 to 16 bits?

Latest Updated: 03/20/2017

Question:

Is it possible to output a synchronous serial signal from the V850 in 16 bits?

Answer:

This depends on how much error is allowed.In a general V850 Series product, this corresponds to repeating 8-bit communications twice.If the CPU processing is fast enough to perform processing between the 1st byte and the 2nd byte, this method can be used.


The V850/SB1 has a serial communication function to enable synchronous communications up to 16 bits in length.If the CPU processing is not fast enough, we recommend you use this model.

Suitable Products
V850 Family