跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Internal Flash memory: what is the corresponding temperature?

Latest Updated:02/27/2012

Question:

For electrical characteristics, there are two kinds of operating ambient temperature at MCU operation time and when Flash writing/erasing. When writing and erasing to an internal Flash memory, which is the corresponding temperature?

Answer:

In CPU rewriting mode, writing and erasing to a Flash memory corresponds to the standard operating ambient temperature when Flash writing/erasing. Flash memory read-out corresponds to the MCU operation standard.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N