跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

In the actual circuit, isn't there an address decoder?

Latest Updated:03/15/2012

Question:

In the port configuration diagram, it looks as though the pin and data bus are connected only through the direction register and port latch. In the actual circuit, isn't there an address decoder?

Answer:

Yes. In order to show multiple ports, we eliminated the address decoder in the diagram.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N