跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

In Tiny series, are there any devices with external address space?

Latest Updated:03/25/2009

Question:

In Tiny series, are there any devices with external address space?

Answer:

There are no devices having external address space since H8/300H Tiny series is a single chip microcontroller.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902