跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to use part of on-chip Flash as a data area?

Latest Updated:03/07/2012

Question:

I want to use part of on-chip Flash as a data area. Can I divide one block into a program area and a data area, and write to and erase each one separately?

Answer:

No, a write is performed in words and an erase is performed in blocks. Therefore, we recommend that the data area and program areas are assigned to separate blocks because the data and programs assigned to one block can be written to but cannot be erased individually.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M16C/62A
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
  • 本文是否實用?