跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to read/write by the external EEPROM using the I2C bus of H8/3664?

Latest Updated:03/24/2009

Question:

I'd like to know how to read/write by the external EEPROM using the I2C bus of H8/3664.

Answer:

Please refer to "Read/Write Access to the On-Chip EEPROM" on the application examples page in this site. Please read the caution before using the application example.

Suitable Products
H8/300H Tiny
H8/3664