跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to execute off -chip memory against performance loss?

Latest Updated:03/23/2009

Question:

Is there anything that can be done against the performance loss, when executing from off-chip memory?

Answer:

Most software spends 90% of its time in only a small number of small inner loops. These could be copied from off-chip memory into on-chip RAM after reset and then be executed there. This way, the performance loss may be almost fully compensated for. Also, some derivatives products have bus controllers that implement countermeasures against the performance loss, e.g. write buffer and burst mode.
Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B