跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the reason of reset caused by the watchdog timer?

Last Updated:12/26/2017

Question:

When "After a reset, count starts automatically" is selected as the count start condition of the watchdog timer, a reset by the watchdog timer will be generated. why?

Answer:

The RAM is also initialized in the start-up file (ncrt0.a30). It might need several tens of milliseconds to initialize the RAM because of the low-speed on-chip oscillator clock divided by 8 is automatically selected as the CPU clock after reset. Therefore, please refresh the watchdog timer in the following macro, too.


====================================================================

; NEAR area initialize.

;--------------------------------------------------------------------

; bss zero clear

;--------------------------------------------------------------------

N_BZERO bss_SE_top,bss_SE

N_BZERO bss_SO_top,bss_SO

N_BZERO bss_NE_top,bss_NE

N_BZERO bss_NO_top,bss_NO



;---------------------------------------------------------------------

; initialize data section

;---------------------------------------------------------------------

N_BCOPY data_SEI_top,data_SE_top,data_SE

N_BCOPY data_SOI_top,data_SO_top,data_SO

N_BCOPY data_NEI_top,data_NE_top,data_NE

N_BCOPY data_NOI_top,data_NO_top,data_NO

Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L