跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How much voltage supply needed to start H8S/21xx F-ZTAT memory devices

Latest Updated:03/23/2009

Question:

What is the voltage supply required to program the H8S/21xx F-ZTAT memory devices.

Answer:

The H8S/21xx (and all H8S FLASH devices) are single rail FLASH programming devices. This means that a 5V devices operates at 5V and requires 5V to program the FLASH. Even though a 3V devices may operate at 5V, it still has to be programmed at 3V.
Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B
  • 本文是否實用?