How much is MCU's current consumption rises when using A/D converter?
Latest Updated:10/10/2008
Question:
(A/D Converter, Electrical Characteristics) How much is the MCU's current consumption increased when using an A/D converter? [2008/10/10]
Answer:
Please refer to the following pages for figures of the A/D converter's current consumption characteristics. Click the Group name of your MCU.
Click:
3823 38D2 38D5 7542 7546 7547 7548 7549
Standard characteristics are example measurements of standard samples. They are provided for reference only and are not guaranteed.
For standard values, please refer to "Electrical Characteristics" in the datasheet for your device. (#107143)
Suitable Products
3803H |
3823 |
3850A |
38D2 |
38D5 |
7545 |
7546 |
7547 |
7548 |
7549 |