跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How high is the current if V850E/MA1 is on reset operation or STOP mode?

Latest Updated:03/19/2017

Question:

How high is the current if V850E/MA1 is on reset operation or STOP mode?

Answer:

How high is the current when the V850E/MA1 (microcontroller) is being a reset operation?
If the reset signal is input continuously, is the current less than that in the HALT or STOP mode?
Suitable Products
V850 Family