How can I distinguish between Spec A and Spec H M38507F8SP/FP part name?
Latest Updated:12/16/2004
Question:
(MCU Comparison, General MPU/MCU) How can I distinguish between Spec.A and Spec.H M38507F8SP/FP with the same part name? [2004/12/16]
Answer:
Spec.A and Spec.H are distinguished by marked serial numbers. For Spec. A, "A" is marked on the left of the serial number.
Ex: A0123456
(#104949)
Suitable Products
3850A |