General registers as 8-bit, 16-bit, 32-bit registers at the same time
Latest Updated:03/26/2009
Question:
Can different general registers be used as 8-bit, 16-bit, and 32-bit registers at the same time?
Answer:
Yes. Registers can be set freely for use as follow.
Suitable Products
H8/300H Tiny |
H8/36109 |
H8/36087 |
H8/36077, H8/36079 |
H8/36064 |
H8/36049 |
H8/36037, H8/36057 |
H8/36014, H8/36024 |
H8/3694 |
H8/3687 |
H8/3672 |
H8/3664 |
H8/36912, H8/36902 |