跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the relationship between HWR, SWR, and WDR in the reset factor determination register (RSTFR)?

Last Updated:12/26/2017

Question:

What is the relationship between HWR, SWR, and WDR in the reset factor determination register (RSTFR)?

Answer:

The bits HWR, SWR, and WDR are exclusive.
When a flag (e.g. HWR bit) is set to 1, other flags (bits SWR and WDR) are set to 0.
Suitable Products
R8C/3x
R8C/5x
R8C/Lx
R8C/Mx