Can transmitted data be outputted when reception overrun error occurs
Latest Updated:03/16/2017
Question:
I am using a serial interface in CSIO mode. Can transmitted data be outputted normally when a reception overrun error occurs during transmission?
Answer:
Even when transmit operation is performed after an overrun error occurred while receiving data, normal transmit data is output. The data written into the SIO transmit buffer register to start the intended transmit operation.
Suitable Products
32170, 32174 |
32171 |
32172, 32173 |
32176 |
32180 |
32182 |
32185 |
32186 |
32192 |
32195 |
32196 |