跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can corresponding standby bit be set to 1 while a function is operating?

Latest Updated:04/05/2011

Question:

While a function is operating, can the corresponding standby bit be set to 1 (standby)?

Answer:

No. Set standby bits to 0 (active) during function operation. Stop the corresponding functions before setting these bits to 1 (standby).
Suitable Products
R8C/2x
R8C/3x
R8C/38A
R8C/Lx
R8C/Mx