跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can a power device be used with the total power dissipation exceeded?

Latest Updated:08/01/2007

Question:

Can a power device be used with the total power dissipation (allowable dissipation) exceeded?

Answer:

No.
If the total power dissipation is exceeded, the chip temperature (junction temperature) exceeds the absolute maximum rating.
Suitable Products
 
  • 本文是否實用?