Can TxDi pin used as an I/O port if transmission is performed in UARTi?
Latest Updated:09/22/2010
Question:
When only transmission is performed using serial interface UARTi, can the RxDi pin used as an I/O port?
Answer:
The RxDi pin can be used as an I/O port.
Suitable Products
M16C/62A |
M16C/62A(M16C/62T) |
M16C/62M |
M16C/62N |
M16C/62N(M3062GF8NFP, M3062GF8NGP) |
M16C/62P |
M16C/63 |
M16C/64A |
M16C/65 |
M16C/6C |
M16C/5L, M16C/56 |
M16C/5LD, M16C/56D |
M16C/5M, M16C/57 |
M16C/30P |
M16C/29 |
M16C/28 |
M16C/26A |