跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can I supply 30mA of current by using the pull-up MOS of each pin for 10mA?

Latest Updated:03/24/2009

Question:

Can I supply 30mA of current by using the pull-up MOS of each pin for 10mA?

Answer:

Yes, You can supply 30mA current by the use of three pins pull-up MOS for 10mA.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power