跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can I monitor the data I am transmitting from the CAN controller ?

Latest Updated:11/12/2008

Question:

Is it possible to monitor the data I am transmitting from the CAN controller ?

Answer:

Yes, by setting bit 1 in the CAN Control register (CiCTLR) the loopback function is invoked and the data transmitted is simultaneously copied to the received message slot.
Suitable Products
R8C/22
R8C/23
M32C/88
M32C/87(M32C/87)
M32C/87(M32C/87A)
M32C/85
M32C/84
M32C/83
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/29
M16C/1N