跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can H8/3048F 5V version operate at 3.3V/8MHz ?

Latest Updated:03/18/2009

Question:

Can H8/3048F 5V version operate at 3.3V/8MHz ?

Answer:

We cannot guarantee 3.3V/8MHz operation of the H8/3048 5V version, as it is not tested or characterised for these parameters.
Suitable Products
H8/300H

 

  • 本文是否實用?