跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are the socket and EXC-180A/SV1 needed between target and option board?

Latest Updated:03/15/2017

Question:

When connecting the target board for the BGA of the V850/SV1, is "EXC-180A/SV1" required between the target board and the option board (emulator)? Also, is the socket for stacking (CSSOCKET180A1513N01S01) required?

Answer:

The sockets required for V850/SV1 (BGA) development are as follows:

EXC-180A/SV1 Emulator connecting pin conversion probe (mandatory)
CSSOCKET180A1513N01S01 Sockets for stacking (for height adjustment; use as required.)
Either CSSOCKET180A1513N01
or CSSOCKET180A1513N01N
is required.
Type with target connection socket guide (A guide hole is required on the board.)

Type without target connection socket guide (No guide hole is required on the board.)
Suitable Products
V850 Family