跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are the H8S/21xx microcontrollers 8 - bit or 16 - bit devices?

Latest Updated:03/23/2009

Question:

Are the H8S/21xx microcontrollers 8 - bit or 16 - bit devices?

Answer:

The H8S/2100 Microcontrollers are one family in the H8S Series of Embedded Microcontrollers. The other H8S families are the H8S/22xx, H8S/23xx and H8S/26xx series. All of these Microcontrollers share the same H8S/2000 CPU Core.  What differentiates theH8S families are the peripherals that are integrated around this common CPU core.  The H8S/2100 series have the same peripherals as the H8/300 Series and as such are ideally suited to these 8 bit applications.
Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B
  • 本文是否實用?