跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are NC pins on H8/300H Tiny Series connected to any internal circuitry?

Latest Updated:03/18/2009

Question:

On the H8/300H Tiny Series are any of the NC pins ( not connected ) actually connected to any internal circuitry of the chip ?

Answer:

No, none of the NC pins are connected to any internal functions on the device. These can therefore be left N/C on your PCB.
Suitable Products
H8/300H Tiny