Any specifications for external capacitor that is connected to port?
Latest Updated:02/27/2012
Question:
Are there any specifications for the external capacitor that can be connected to the port?
Answer:
The value of the external capacitor is not specified. However, when shutting down the MCU power please note that the voltage applied to the port should not be higher than the power supply voltage.
Suitable Products
M32C/8A |
M32C/88 |
M32C/87 |
M32C/85 |
M32C/84 |
M32C/83 |
M32C/80 |
M16C/62A |
M16C/62A(M16C/62T) |
M16C/62M |
M16C/62N |
M16C/62N(M3062GF8NFP, M3062GF8NGP) |
M16C/62P |
M16C/63 |
M16C/64A |
M16C/64C |
M16C/65 |
M16C/65C |
M16C/6C |
M16C/6N4, M16C/6N5 |
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN |
M16C/5L, M16C/56 |
M16C/5LD, M16C/56D |
M16C/5M, M16C/57 |
M16C/30P |
M16C/29 |
M16C/28 |
M16C/26A |
M16C/1N |