跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(Pin) What is the initial output level of CNTR1 output? [2007/08/09]

Latest Updated:08/09/2007

Question:

(Pin)  What is the initial output level of CNTR1 output? [2007/08/09]

Answer:

The initial output level of CNTR0 output is high impedance.
When the P11/CNTR0 pin function selection bit (W63) is set to 0, the value of the port P11 output latch is output from the pin.
However, internally, CNTR0 output will be in the initial high impedance state. (#106690)
Suitable Products
4508
4509