跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(M32C) What happens to count source when CPU clock is changed?

Latest Updated:09/22/2010

Question:

When a CPU clock is changed from a main clock to an on-chip oscillator clock, what happens to the count source of the peripheral function?

Answer:

The on-chip oscillator clock becomes the count source of the peripheral function. However, the count sources of peripheral functions that were set to f2n(1) or fC32 will be unchanged.
Note:

  1. When XIN clock (fXIND) is selected as f2n count source
Suitable Products
M32C/80
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80