跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(M16C,M32C) Are there any hardware precautions for accurate A/D conversion?

Latest Updated:02/27/2012

Question:

Are there any hardware precautions for realizing accurate A/D conversion?

Answer:

In order to perform A/D conversion, it is necessary to fully charge the internal capacitor, but if the impedance of the A/D conversion target is high, the discharge and charge will take time and the conversion value will not be accurate. For correct A/D conversion, please set the impedance of the signal source connected to the analog input pin so that it is low enough. (Refer to the hardware manual for the calculation method.) Moreover, in order to suppress the influence of the input current at the time of A/D conversion, please add a capacitor to the analog input pin.

Example (M16C/62P)

[ About the R8C Family products, click here.]

Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N