跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(Interrupts) How long is the interrupt delay? [2005/03/01]

Latest Updated:03/01/2005

Question:

(Interrupts)   How long is the interrupt delay? [2005/03/01]

Answer:

Please refer to the following figures.
Basically, it takes from 7 to 23 cycles from the generation of the interrupt request to the actual execution of the interrupt processing routine, as elaborated below:

  • Main Routine 0 - 16 cycles
    Varies according to instruction execution status.
    0 cycles: just as instruction is completed,
    16 cycles: just as DIV instruction is started
  • Waiting time for post-processing of pipeline : 2 cycles fixed
  • Stack push, Vector fetch : 5 cycles fixed

(#104774)

 

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549