跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(3850A) What values of external capacitance can be added to the ports?

Latest Updated:10/26/2006

Question:

(I/O Port)  What values of external capacitance can be added to the ports ? [2006/10/26]

Answer:

(1) CMOS3 State I/O Ports
When adding external capacitance, select 100pF or less.

(2) Input-only Ports
There are no special restrictions on these ports. Select the capacitance according to the characteristics of the externally connected circuit.
(#104751)

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549