跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the value of the thermal resistance of the FP-64E package ?

Latest Updated:03/18/2009

Question:

What is the value of the thermal resistance of the FP-64E package ?

Answer:

The thermal resistance between contact and case: jc = 33 degrees Celsius/W The thermal resistance between contact and peripherals: ja = 116 degrees Celsius/W (mounted on board).
Suitable Products