跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the quantity of materials of pins of lead free products?

Latest Updated:06/01/2007

Question:

What is the quantity of materials other than Sn contained in solder with which the pins of lead-free products are plated?

Answer:

The packaging of lead-free products includes:
Sn-Bi: Approx. 2wt% of Bi
Sn-Ag-Cu: Approx. 3wt% of Ag and 0.5wt% of Cu

Please see our Lead-Free Semiconductor Products pamphlet for details.
Suitable Products
  • 本文是否實用?