跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can U of UPD*** be taken as μ?"

Latest Updated:11/01/2005

Question:

A customs officer asked "A product name is printed on the label of the packing box as 'UPD***', but the parameter sheet says 'μPD***'. In this case, U of UPD*** can be taken as μ?"

Answer:

Yes. U is used because the keyboard of a PC does not have μ and most IT systems cannot use μ.
Suitable Products