跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are SC-62 and SOT-89 the same?

Latest Updated:04/01/2007

Question:

Are SC-62 and SOT-89 the same?

Answer:

SC-62 is the name given by the Electronic Industries Association of Japan (EIAJ) and SOT-89 is the name given by Joint Electronic Device Engineering Council (JEDEC, an American industrial organization) that promotes standardization of electronic components). Although the names differ, the package shapes are the same.
Suitable Products