跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Full-Duplex Communication/Half-Duplex Communication [Common Content]

Last Updated:05/25/2018

Question:

Full-duplex communication/half-duplex communication [common content]

Answer:

• Full-duplex communication method
 Bidirectional communication method that enables simultaneous communication by using two sets of single-directional communication channels
 (e.g., UART, SPI, and CSI)

• Half-duplex communication method
 Bidirectional communication method that uses a single set of bidirectional communication channels and switches between sending and receiving
 Although the communication speed is slower than that in full-duplex communication, the number of communication channels can be reduced.

Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C
78K Family
  • 本文是否實用?