跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Does Vector Interrupt Processing Run per Subsystem Clock

Last Updated:05/25/2018

Question:

After the system enters the HALT mode while the subsystem clock is running but the main system clock is stopped, if this mode is canceled using an unmasked interrupt, vector interrupt processing occurs. Does this vector interrupt processing run according to the subsystem clock as it is?

Answer:

Yes, vector interrupt processing will run according to the subsystem clock as it is.
Note that even if you cancel the HALT mode by using an unmasked interrupt, that does not guarantee that vector interrupt processing will be executed.
If the CPU is in the DI state, the HALT mode will be simply canceled and no vector processing will be executed.
Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C
78K Family